GPMI- Where does my recieved data end up?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPMI- Where does my recieved data end up?

962 次查看
briannorman
Contributor II

I'm working on an iMX6 GPMI interface to an asynchronous NAND flash.  Taking baby steps, I have been able to issue a reset to the chip and now I'm trying to read it's id.  The ID is 5 bytes long and when i set up the dma chain, I see that it actually respond with the right id, but the data is never moved to my buffer.  I see the last byte in the GPMI_DATA register, and if i change my dma number of bytes to recieve to 4, i see the first 4 bytes so i know that the GPMI is recieving the data from the NAND.  Also, the GPMI_STAT shows that the fifo is empty(bit2).  So, where did my data go?

I set the GPMI_PAYLOAD to point to a static local variable, made sure it was word aligned, but nothing shows up there.  I had some difficulties initially until i realized that the address registers all needed to be actual addresses, not the mapped address i am used to looking at, but once i changed all addresses by the offset that they are mapped to, my DMA command word chains work great.  I'm puzzled because my DMA Read commands work fine, i used a similar local variable to store all my commands and just point the DMA buffer to them, with the offset.  It appears that the DMA write isn't working. 

Any suggestions, am i even looking at the right place?  What could cause my DMA write to not write, but not report any errors?

标签 (2)
0 项奖励
回复
0 回复数