GPIO handling after shutdown IMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO handling after shutdown IMX6ULL

ソリューションへジャンプ
1,371件の閲覧回数
amiraj_patel
Contributor I

hello,

we are using the IMX6ull Processor and used with our device and we want to add the power/reset switch to the device.

we are using yocto image dunfell.

so for graceful shutdown we have used the command "shutdown -h now"

after the successful execution all peripherals and interfaces are disabled but however the GPIO still hold it's state,

1. is there any way to shutdown and also clear the GPIOs after executing shutdown ? 

2. if yes, how we can do so ?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,301件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @amiraj_patel!

 

I am not sure if that switch can be implpemented in the toradex board.

 

I recommend contacting Toradex Support.

 

https://community.toradex.com/

 

Best Regards!

Chavira

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,346件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @amiraj_patel!

 

Thank you for contacting NXP Support!

 

By default when you turn off the processor all ports are turned off too.

 

For this case I recommend the next:

 

1) Check your power on/off sequence and compare it with the datasheet.

 

2) Check your schematic and see how is connected your LED to the processor.

if is possible share your schematic.

 

Best Regards!

Chavira

0 件の賞賛
返信
1,320件の閲覧回数
amiraj_patel
Contributor I

we are using right now the imx6ull of Toradex,

here is the link for some and the carrier board

SOM - https://www.toradex.com/computer-on-modules/colibri-arm-family/nxp-imx6ull?utm_term=imx6ull&utm_camp...

Carrier Board - https://www.toradex.com/products/carrier-board/viola-carrier-board?srsltid=AfmBOop7Ua0jZdnIPaAIB_9te...

I want to use one GPIO as a Power on/off button and the GPIO needs to be clear after a successful shutdown operation.

and I also want the functionality of power on with the same can you suggest anything?

we are planning to use the power kill switch - https://www.analog.com/media/en/technical-documentation/data-sheets/2954fb.pdf

let me know if there are any other details you want to know.

0 件の賞賛
返信
1,302件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @amiraj_patel!

 

I am not sure if that switch can be implpemented in the toradex board.

 

I recommend contacting Toradex Support.

 

https://community.toradex.com/

 

Best Regards!

Chavira

0 件の賞賛
返信