GPIO config register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO config register

1,888 Views
xu_ji1
Contributor V

Hello,

Could u help detail explain about GPIO config below:

update_mux_mode
update lock for mux control
write 1 to allow programming to mux control [29:19]

update_pad_ctl
update lock for pad control
write 1 to allow programming to pad control [14-1:0]

Just for little words I can not understand it more,when set the register 1 and when set 0?

pls help it

Thanks

0 Kudos
Reply
2 Replies

560 Views
flobro
Contributor IV

I am using the iMX8 Quad Max, and I have seen examples of gpio settings where those bits are not used, but the bits they alledgedly control are modified. The information supplied is not a solution, the documentation does not appear to say if/when it needs to be used.

Could someone please explain if/when the update_mux_mode and udate_pad_ctrl need to be used?

0 Kudos
Reply

1,619 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

one can check sect.2.1.5.6 IOMUX Control Through GPIO Module attached Linux Manual and

sect.Chapter 8 Configuring IOMUX Porting Guide from nxp software documentation link below

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

For i.MX8 series use SCFW documentation in SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply