Hi ,
I am working on i.MX8 DX6 board where I am facing issue in toggling few GPIOs from GPIO 0 bank such as GPIO_04 , GPIO_05 , GPIO_07 . I have tried changing the drive strength of the GPIO's in pad settings but that did not solve the issue.
When the GPIO's are made to toggle from the uboot, the data register of the corresponding GPIO's are getting reflected with the updated value but the GPIO's are in their default state when probed .
I tried to configure the pads in the SC firmware code and tried to toggle the GPIOs. But the Issue persists.
Only these three GPIOs are not being able to control through software and the other GPIO's in the same bank are toggling.
And interesting part is ,in i.MX8QXP board , these three GPIO's are working fine .
Attaching the CRO captured images of GPIO_4 toggling in QXP and DX6 board.
Any one faced similar issue in i.MX8 DX6 board.?
Any help would be appreciated
Hi Igor,
Thank You for the reply .
I looked into SCFW documentation . But my doubts still not cleared . Let me elaborate it once again.
The GPIO 4 configured to ESAI0_TX0 pad , GPIO 5 configured to ESAI0_TX1 pad and GPIO 7 configured to ESAI0_TX2_RX3 pad requires IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB pad to be configured for toggling. But the GPIO 3 which is configured to ESAI0_SCKT pad still toggles without any extra settings. Even though all the GPIO's belong to a same pad group [ESAI0], each pins require different settings . As you answered some pads are dual voltage pads and some other single voltage pads. But basically these pins under this pad group supports 1.8 ,2.5 and 3.3 Voltage [VDD_ESAI_SPDIF_1P8_2P5_3P3] and our hardware team has fixed the voltage to 1.8 V for the 10 pins under this ESAI0 pad group.
So my question is , how one can identify the ESAI0_TX0,ESAI0_TX1,ESAI0_TX2_RX3 pads belong to dual voltage support pads and require IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB pad to be configured while ESAI0_SCKT is single voltage pad?
Hi Igor,
This was the field I strongly hoped to indicate the single and dual voltage support .But I can find the PDRV field with 1.8 and 3.3v voltage support under ESAI0_SCKT pad too and ESAI0_SCKT is a single voltage supporting pad according to the findings till now.
Thanks & Regards,
Anjali
regarding "extra settings", rev.B0 sets PSW_OVR for ENET segment to
1'b1 by default (2.5V) and since ESAI0_TX0, ESAI0_TX1,ESAI0_TX3_RX2 are used for
ENET1 so GPIORHB field PSW_OVR should be set to 0 for 1.8/3.3V operation.
Best regards
igor
Hi Igor,
Thank You for the support and reply.
In your last reply since you have mentioned "rev.B0" particularly , I am concluding my second question
Whether these settings are required only for iMx8DX6 (B0 silicon)?
as answered to be yes.
After referring the fsl-imx8qxp-lpddr4-arm2.dts file ,
pinctrl_fec2: fec2grp {
fsl,pins = <
SC_P_ESAI0_SCKR_CONN_ENET1_RGMII_TX_CTL 0x00000060
SC_P_ESAI0_FSR_CONN_ENET1_RGMII_TXC 0x00000060
SC_P_ESAI0_TX4_RX1_CONN_ENET1_RGMII_TXD0 0x00000060
SC_P_ESAI0_TX5_RX0_CONN_ENET1_RGMII_TXD1 0x00000060
SC_P_ESAI0_FST_CONN_ENET1_RGMII_TXD2 0x00000060
SC_P_ESAI0_SCKT_CONN_ENET1_RGMII_TXD3 0x00000060
SC_P_ESAI0_TX0_CONN_ENET1_RGMII_RXC 0x00000060
SC_P_ESAI0_TX3_RX2_CONN_ENET1_RGMII_RXD1 0x00000060
SC_P_ESAI0_TX2_RX3_CONN_ENET1_RGMII_RXD2 0x00000060
SC_P_ESAI0_TX1_CONN_ENET1_RGMII_RXD3 0x00000060
>;
};
From the above code snippet , the ESAI0 pad is used for ENET1 as you said.But the ESAI0_SCKT is also used for ENET1. But the ESAI0_SCKT is still controllable without GPIORHB pad setting.
Thanks & Regards,
Anjali
Hi Anjali
yes this is applicable only for B0 revision. I believe ESAI0_SCKT is already configured
as rgmii output so it may be controllable without additional GPIORHB pad setting.
Best regards
igor
Hi Anjali
one can apply to local marketing office for more details.
Note this part is still as "PREPRODUCTION", that is not fully supported.
i.MX 8X Applications Processors| Arm® Cortex®-A35, Cortex-M4 | NXP
Best regards
igor
Hi Igor,
Thank You for the reply.
I had gone through the chapter 9 of the reference manual and came across " Single voltage and dual voltage pad " .
How can we identify whether the pad belongs to single voltage or dual voltage?
I am still going through the reference manual for identifying the single voltage and dual voltage pads.
Thanks & Regards,
Anjali
Hi Anjalik
you can find answer yourself looking at your post with:
"IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB pad".
So you can look in scfw documentation for that pad API's.
Best regards
igor
Hi Anjalik
based on waveforms and that when part was emulated on i.MX8QXP MEK platform
there were no such issues, seems this is custom board hardware problem :
poor soldering or shorting to gnd/other signals. One can recheck board layout
and perform x-ray screening.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
After configuring the IOMUXD_COMP_CTL_GPIO_1V8_3V3_GPIORHB pad in the uboot source code the GPIO 4 , 5,7 under GPIO 0th bank started toggling. I still have few queries on this
Why pad control setting is necessary for few GPIO pins?
Whether these settings are required only for iMx8DX6 (B0 silicon)?
It would be great if these doubts are clarified. Awaiting for your reply.
Thanks & Regards,
Anjali
Hi Igor,
Thanks for the reply.
We have done x-ray screening for a board from the assembly house and it is fine. We are facing this issue in all the boards so I think we can rule out the possibility of poor soldering or shorting to gnd/other signals.
Is there anything specifically to be taken care while designing the custom board based on i.MX8DX6 with respective to GPIOs?