GPIO R/W speed far below the set kCLOCK_RootIpg (133 Mhz)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO R/W speed far below the set kCLOCK_RootIpg (133 Mhz)

2,882 Views
Chengting
Contributor II

We'd plan to use GPIO4 for data transfer(i.MX8P dual core) . Thus we gave a test of the GPIO speed.

M7 part test.

//skipping the iomux setting and pin setting

while (i<100 000 000)

{

     //read

     GPIO_PinRead(GPIO4,0);

     //pulling high
     GPIO_PinWrite(GPIO4,18,1);
 
     //pulling low
     GPIO_PinWrite(GPIO4,18,0);
      i++;
}

It cost 33 s, totally, the speed is far behind the IPG_clk we set, 133Mhz.

1696055385.jpg

As the image show, every high last 65 ns, every repeat last 330 ns.

If the read cost 2 clock loop, the clock time is 30 ns, which is 33Mhz, far behind the 133 hHz in reference Manual.

Chengting_0-1679215423978.png

Chengting_1-1679215601172.png

 

 

0 Kudos
Reply
4 Replies

2,827 Views
Chengting
Contributor II

Thanks for your reply. How do I know the correct speed (or the highest speed the platform can support)?

That's what I really really need. Thank you again.

static inline uint32_t GPIO_PinRead(GPIO_Type *base, uint32_t pin)
{
    assert(pin < 32U);

    return (((base->DR) >> pin) & 0x1U);
}

void GPIO_PinWrite(GPIO_Type *base, uint32_t pin, uint8_t output)
{
    assert(pin < 32U);
    if (output == 0U)
    {
#if (defined(FSL_FEATURE_IGPIO_HAS_DR_CLEAR) && FSL_FEATURE_IGPIO_HAS_DR_CLEAR)
        base->DR_CLEAR = (1UL << pin);
#else
        base->DR &= ~(1UL << pin); /* Set pin output to low level.*/ //==> this branch
#endif
    }
    else
    {
#if (defined(FSL_FEATURE_IGPIO_HAS_DR_SET) && FSL_FEATURE_IGPIO_HAS_DR_SET)
        base->DR_SET = (1UL << pin);
#else
        base->DR |= (1UL << pin);  /* Set pin output to high level.*/  //==> this branch
#endif
    }
}

 

0 Kudos
Reply

2,808 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Chengting ,

 
I hope you are doing well.
 
The correct gpio togging speed is not documented anywhere as it depends upon many things and overheads of applications can also affect it.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

2,855 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @Chengting 

I hope you are doing well.
 
The clock source for gpio modules is ipg_clk_s (Clock root: IPG_CLK_ROOT).
 
Here, ipg_clk_s is used for synchronization in gpio sampling, reading register values, etc...
It does not mean the frequency at which gpio output toggles in this example.
 
This test does have the overhead of other instructions (loop condition, increment,).
 
GPIO_PinWrite() function also contains various conditional branching.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply

2,821 Views
Chengting
Contributor II

Thanks for your reply. How do I know the correct speed (or the highest speed the platform can support)?

That's what I really really need. Thank you again.

static inline uint32_t GPIO_PinRead(GPIO_Type *base, uint32_t pin)
{
    assert(pin < 32U);

    return (((base->DR) >> pin) & 0x1U);
}

void GPIO_PinWrite(GPIO_Type *base, uint32_t pin, uint8_t output)
{
    assert(pin < 32U);
    if (output == 0U)
    {
#if (defined(FSL_FEATURE_IGPIO_HAS_DR_CLEAR) && FSL_FEATURE_IGPIO_HAS_DR_CLEAR)
        base->DR_CLEAR = (1UL << pin);
#else
        base->DR &= ~(1UL << pin); /* Set pin output to low level.*/ //==> this branch
#endif
    }
    else
    {
#if (defined(FSL_FEATURE_IGPIO_HAS_DR_SET) && FSL_FEATURE_IGPIO_HAS_DR_SET)
        base->DR_SET = (1UL << pin);
#else
        base->DR |= (1UL << pin);  /* Set pin output to high level.*/  //==> this branch
#endif
    }
}
Tags (1)
0 Kudos
Reply