Hi,
I am working on IMX8M MINI EVK on linux environment ,i have added an MX8MM_IOMUXC_SAI5_RXD2_GPIO3_IO23 pin in the imx8mm.dts file and i have compiled the device file using # bitbake -c compile -f linux-imx and # bitbake -c deploy -f linux-imx later i have flashed the image into the sd card then i"m checking for the 88 pin in the cat/sys/class/gpio section ,I'm unable to see the pin .How to get the pin into kernel.