GPIO Electrical Characteristics on i.MX6 SOLO

cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO Electrical Characteristics on i.MX6 SOLO

140 Views
martindenion
Contributor II
I would like to know more about the electrical characteristics of GPIO1_18 on the i.MX6 SOLO processor like maximum input current and maximum voltage.
0 Kudos
5 Replies

122 Views
martindenion
Contributor II

Okay thanks, but why are there 3 "Typ" voltages for these GPIOs? Can we put any of these 3 or they are GPIO with "programmable" voltage?

0 Kudos

111 Views
IvanRuiz
NXP TechSupport
NXP TechSupport

Hello,

 

You can put any you want to; the "typ" values mean that they are the typical value for the listed voltage rails within the range (from 1.65 to 3.6V) that you can select from.

 

BR,

Ivan.

0 Kudos

132 Views
IvanRuiz
NXP TechSupport
NXP TechSupport

Hello,

 

For the GPIO DC Parameters, please refer to table 4.6.2, and for the voltage rails for GPIO supply voltages, please refer to table 8 of the datasheet, which in this case, NVCC_SD1 corresponds to the GPIO1_IO18: https://www.nxp.com/docs/en/data-sheet/IMX6SDLIEC.pdf

 

Hope it helps!

 

BR,

Ivan.

0 Kudos

106 Views
martindenion
Contributor II

Thank you! I have two more questions regarding Table 4.6.2:

I don't understand why the IO current limit for these GPIOs is lower when Vin=0V than when Vin=OVDD.

Moreover, if I want to connect one of these GPIOs to a pullup resistor with for example a voltage of 1.8V and I want to limit the current (as written in the table) to 1µA, does it mean that this pullup resistor should have a value of 1.8M? This value seems strange.

0 Kudos

100 Views
IvanRuiz
NXP TechSupport
NXP TechSupport

Hello,

 

No, for the maximum supply currents, please refer to table 10 of the datasheet: https://www.nxp.com/docs/en/data-sheet/IMX6SDLIEC.pdf

 

BR,

Ivan.

0 Kudos