G2D function between 8M Quad and 8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

G2D function between 8M Quad and 8M Plus

749 Views
hankwang
Contributor V

Hi,

   We have a screen capture program that transmits the screen over the network ( like remote desktop). The program runs on the 8MP CPU, the CPU usage will be 97%. The program runs on the 8MQ CPU, the CPU usage will be 82%. When we enable the g2d function on the 8MP , the CPU usage will be 80-82% .

 Why the 8MQ CPU not need to enable g2d function, the CPU usage rate is still relatively low? 

Labels (1)
0 Kudos
Reply
1 Reply

745 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hank

 

CPU usage rate may be low due to larger L2 cache, 1MB vs 512KB in 8M Plus.

 

Best regards
igor

 

 

0 Kudos
Reply