Future Electronics Presentations at Americas FTF 2010

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Future Electronics Presentations at Americas FTF 2010

724件の閲覧回数
iafg
Contributor IV
Future demonstrated their new Panel Interface Module (PIM) for i.MX development kits. The PIM allows for rapid interfacing and evaluation of TTL and LVDS panels with most of the existing i.MX EVKs and PDKs. It is a small board that plugs into the Standard Conector found on these boards. An LVDS tranciever is on board, and the connectors mate with quickly-customizable Quadrangle cables available through Future. The Quadrangle cables are made to interface with the display under evaluation.

The attached pictures show the PIM running on an i.MX25 EVK driving a 5.7"TTL display, and on an i.MX31 driving an 10.4" LVDS display (as well as the original EVK display)

For more information please contact your local Future Electronics sales.
タグ(1)
0 件の賞賛
返信
0 返答(返信)