Fusing MAC address for MX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fusing MAC address for MX8MP

跳至解决方案
2,832 次查看
khang_letruong
Senior Contributor III

Dear Experts,

I would like to fuse the MAC address for our customized MX8MP based board. I found certain discussion about this subject such as the following : https://community.nxp.com/t5/i-MX-Processors/imx8m-plus-fuse/m-p/1270171. In this discussion, the author used : 

u-boot=> fuse prog -y 9 0 0xeeff

u-boot=> fuse prog -y 9 1 0xaabbccdd

but  I read back incorrect value. as below. 

Word 0x00000000: ffdfbfaf
u-boot=> fuse read 9 1
Reading bank 9:

Word 0x00000001: 072fffff

However, I wonder where to find reliable info about the bank number as well as bytes' order in word value, please ?

Thanks a lot and hope to hear from you,

Khang

 

0 项奖励
回复
1 解答
2,764 次查看
b36401
NXP Employee
NXP Employee

Yes, fuse locks are shared between MAC addresses.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,828 次查看
b36401
NXP Employee
NXP Employee

Please check MAC fuse lock bit.

0 项奖励
回复
2,812 次查看
khang_letruong
Senior Contributor III

Dear @b36401 ,

 

Thanks for your advice but it's still vague for me, especially in the case that I need to program the fuse of the 2nd Ethernet interface (EQoS, index 1) and the words reserved for MAC addresses seem to be shared btw the 2 MAC addresses.

Best regards,

Khang

 

标记 (1)
0 项奖励
回复
2,765 次查看
b36401
NXP Employee
NXP Employee

Yes, fuse locks are shared between MAC addresses.

0 项奖励
回复