Fusemap of i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fusemap of i.MX6SL

Jump to solution
1,568 Views
ko-hey
Senior Contributor II

Hi all,

Let me know a fusemap of i.MX6SL.

Is the fusemap of i.MX6SL same as i.MX6Q/D ?

For example, according to the IMX6DQRM, BOOT_CFG3[6] is BT_MMU_DISABLE.

Is it same as i.MX6SL ?

Ko-hey

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,289 Views
b36401
NXP Employee
NXP Employee

Actually the fusemaps of i.MX 6SL and i.MX 6Q/D series are different.

For more details regarding to fusemap you can refer chapter 5 "Fusemap"

of i.MX 6SoloLite Applications Processor Reference Manual.

As for BT_MMU_DISABLE bit you are asking about, it is located at 0x470 not in BOOT_CFG3.

Please look at the bottom of page 244 of that document.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,290 Views
b36401
NXP Employee
NXP Employee

Actually the fusemaps of i.MX 6SL and i.MX 6Q/D series are different.

For more details regarding to fusemap you can refer chapter 5 "Fusemap"

of i.MX 6SoloLite Applications Processor Reference Manual.

As for BT_MMU_DISABLE bit you are asking about, it is located at 0x470 not in BOOT_CFG3.

Please look at the bottom of page 244 of that document.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,289 Views
ko-hey
Senior Contributor II

Hi Victor

Sorry, I was overlooking it.

Thanks.

Ko-hey

0 Kudos
Reply