Fusemap of i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fusemap of i.MX6SL

跳至解决方案
1,031 次查看
ko-hey
Senior Contributor II

Hi all,

Let me know a fusemap of i.MX6SL.

Is the fusemap of i.MX6SL same as i.MX6Q/D ?

For example, according to the IMX6DQRM, BOOT_CFG3[6] is BT_MMU_DISABLE.

Is it same as i.MX6SL ?

Ko-hey

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
752 次查看
b36401
NXP Employee
NXP Employee

Actually the fusemaps of i.MX 6SL and i.MX 6Q/D series are different.

For more details regarding to fusemap you can refer chapter 5 "Fusemap"

of i.MX 6SoloLite Applications Processor Reference Manual.

As for BT_MMU_DISABLE bit you are asking about, it is located at 0x470 not in BOOT_CFG3.

Please look at the bottom of page 244 of that document.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
753 次查看
b36401
NXP Employee
NXP Employee

Actually the fusemaps of i.MX 6SL and i.MX 6Q/D series are different.

For more details regarding to fusemap you can refer chapter 5 "Fusemap"

of i.MX 6SoloLite Applications Processor Reference Manual.

As for BT_MMU_DISABLE bit you are asking about, it is located at 0x470 not in BOOT_CFG3.

Please look at the bottom of page 244 of that document.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
752 次查看
ko-hey
Senior Contributor II

Hi Victor

Sorry, I was overlooking it.

Thanks.

Ko-hey

0 项奖励
回复