Hi,
I am designing the USBs for imx8mp using only 2.0 phy D+ and D-, because I do not need usb 3.0.
One USB is connected to 2.0 hub in the pcb, so always will be a host. The other is used as micro USB otg connector that can be host or device.
I have some doubts about USBx_VBUS pins:
What is the function of USB1_VBUS (ball A11) and USB2_VBUS (ball D12)?
In the case of USB HUB connection: could be this pin floating?
In the case of USB micro OTG connector: this pin needs to be connected to 5V of the USB OTG connector?