Function of EMI pin keeper for i.MX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Function of EMI pin keeper for i.MX28

2,289 Views
ko-hey
Senior Contributor II

Hi all

 

Let me confirm about a function of "Keeper” which is described in reference manual.

I'm confused about that.

 

Q1.

There are two words which are very similar.

One is "Internal Keeper”, the other is "Pad keeper”.

Is it same meaning ?

 

Q2.

There are following description in 9.1 Pin Control and GPIO Overview.

 

"All EMI pins' internal keepers can be disabled to allow them to change to a highimpedance

state (as required by some DRAM manufacturers).”

 

How can I judge whether DRAM manufactures require a high impedance state or not ?

 

 

Ko-hey

 

Labels (1)
0 Kudos
Reply
5 Replies

2,023 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.
  IMX28 digital pins have internal keepers, which are configured,
using PINCTRL Pad Keeper Disable Registers.

2.
 Use DRAM specs, provided in Datasheets, regarging high impedance
requirements.

Regards,

Yuri.

0 Kudos
Reply

2,023 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

> Use DRAM specs, provided in Datasheets, regarging high impedance requirements.

Could you show me an example for it ?

Ko-hey

0 Kudos
Reply

2,023 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I have not found the mentioned requirements about high impedance in 

Datasheets for the following DRAM devices, that can be used with i.MX28:

MT46H64M16 and EDE1116AEBG.

Regards,

Yuri.

0 Kudos
Reply

2,023 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

I found a description which is written as required specification in P10 of following document .

http://www.samsung.com/global/business/semiconductor/file/product/ddr-device_operation_timing_2002_1...

I think it's a requirements about high impedance.

Am I correct ?

Furthermore, do you have any document for internal circuit when user set internal keeper to disable ?

I can't figure out what kind of difference will occur internally when I disable it.

Ko-hey

0 Kudos
Reply

2,023 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the mentioned specs (from Samsumg) are standard requirements for DRAM signals during 

operations, when data bus state should be dynamically changed. The i.MX28 keeper option 

are used to configure pin's state for relatively long time (statically). As general example, it makes

sense for multi-master system, when one master should free bus for others.    

  Hope the following tutorial helps to understand keeper operation.

http://www.ti.com/lit/an/scla015/scla015.pdf 

Regards,

Yuri.

0 Kudos
Reply