Full usage of VPU , GPU and IPU of imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full usage of VPU , GPU and IPU of imx6

2,084件の閲覧回数
abeeshmp_dct
Contributor II

Hi Team, 

For a product we are using the imx6 quad to capture the video frames using the CSI, convert it to RGBA format using the gpu and also render some overlay frames on top of the camera video by using the GPU again and then convert it to 420 format by IPU and feed it to VPU ( h264) for getting encoded to stream over network.

In this scenario, if we use 1280x1024@30fps, all seems working well, but if we increased the fps to 50, then vpu takes much more time to encode( it was taking 25 ms for 30fps case, now it takes around 50ms).

But if we reduce the GPU load by avoiding overlay rendering , then at the same 50fps, VPU takes only around 25ms itself. 

That means, VPU peroformance is affected by the GPU load?

Is there any way to avoid this dependency between VPU and GPU performance?

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,075件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello abeeschmp,

 

The only solution is to try to reduce the memory with VPUmem or GPUmem to see if let you get the fps that you need.

 

Regards

0 件の賞賛
返信

2,033件の閲覧回数
abeeshmp_dct
Contributor II

Hello Bio_TICFSL

Thanks for the reply. Could you please explain more on that ? You mean to reduce the resolution to get higher fps  or something other? 

 

0 件の賞賛
返信