From ATK to MFG - How to flash iMX25 NAND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

From ATK to MFG - How to flash iMX25 NAND

1,427 Views
alessandroa_
Contributor I

Dear all,

I always used successfully ATK to flash NAND type (MT29F1G16) on my iMX25 device with MQX RTOS

Now, in order to make it possible also on Win 7/8,

I need to migrate to MFG tool.

Device is correctly recognized as Freeescale i.MX25 BulkIO Device

But something goes wrong during

"push" operation (UTP mode) ---- > error code=-65520

or

"program" operation (RKL mode) ---- > Updater Error -22136

UCL attached.

- "mx25_nand.bin" is my micro-loader image used with ATK

- "Bootloader.bin" is the module I want to flash starting from 0x00000000

- "mx25ddr2.xml" is the memory file used also with ATK

Any idea about how to fix it?

Many thanks in advance

Regards,

Alessandro A.

- UTP mode:

<UCL>

  <CFG>

    <STATE name="BootStrap" dev="MX25" />

    <DEV name="MX25" vid="15A2" pid="003A"/>

  </CFG> 

  <LIST name="NAND" desc="Choose Nand as media">

    <CMD type="find" body="BootStrap" timeout="60"/>

    <CMD type="init" body="Memory" file ="mx25ddr2.xml" />

  <CMD type="load" file="Bootloader.bin" address="0x70100000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Doing preLoad."</CMD>

  <CMD type="load" file="mx25_nand.bin" address="0x80800000" loadSection="OTH" setSection="APP" HasFlashHeader="TRUE" >Loading OS image.</CMD>

    <CMD type="jump" > Jumping to OS image. </CMD>

  <CMD type="push" body="send" file="files/Bootloader.bin">Sending Bootloader.bin</CMD>

  </LIST>

</UCL>

- RKL mode:

<UCL>

  <CFG>

    <STATE name="BootStrap" dev="MX25" />

    <STATE name="RamKernel" dev="MX25" />

    <DEV name="MX25" vid="15A2" pid="003A" />

  </CFG>

  <LIST name="NAND" desc="Program FW into flash">

  <CMD type="rklCmd" body="FlashInit" timeout="120" />

  <CMD type="init" body="Memory" file ="mx25ddr2.xml" />

    <CMD type="program" file="Bootloader.bin" address="00000000" readback="TRUE" />

  </LIST>

</UCL>

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

852 Views
Yuri
NXP Employee
NXP Employee

  Strictly speaking, the  micro-loader image "mx25_nand.bin", used with ATK,
cannot be used with the MFG.

You may find MFG configuration for i.MX25 in Community.

“MX25 3stack HAB (High Assurance Boot)”
https://community.freescale.com/docs/DOC-94911

“How to create your own Mfgtool firwmare”

https://community.freescale.com/message/408920#408920


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply