Fresh Imx6q custom board always I serial Downloader mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fresh Imx6q custom board always I serial Downloader mode

1,631件の閲覧回数
venkatachilakal
Contributor III

I am working on a imx6q based custom board. The configuration is similar to Sabre SD board.  

When  I make boot options  as 00 still my board is detected as HID DEVICE in my host pc.  As I did the same thing with Sabre lite development board it is not detecting.. 

My question is,  when the processor and emmc are new is that board will always goes into serial Downloader mode? 

ラベル(2)
2 返答(返信)

1,311件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi VENKATA

please check sect.8.2.3 Boot From Fuses Mode (BOOT_MODE[1:0] = 00b) i.MX6DQ RM

http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf 

If set to Boot From Fuses, the boot flow is controlled by the BT_FUSE_SEL eFUSE
value. If BT_FUSE_SEL = 0, indicating that the boot device (for example, Flash, SD/
MMC) has not yet been programmed, the boot flow jumps directly to the Serial
Downloader.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,311件の閲覧回数
venkatachilakal
Contributor III

Thank you very much for your reply...  

I have an other question that even if I set my boot mode 10 ( board configuration),  my board is still in serial Downloader mode. 

Any thing wrong can be happen..?

0 件の賞賛
返信