Frequent hardfault on startup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Frequent hardfault on startup

跳至解决方案
2,843 次查看
Daan
Contributor III

Hello,

 

On an RT1064 I run a FreeRTOS based project. Quite frequent the application will not startup from the debugger because of a hardfault, if I reflash the application, it works properly (I didn't change the application nor do I need to recompile it). If I inspect the call stack, it is very random where the error originated, it can be USB, ethernet, File system, but it's always some FreeRTOS sourcefile, but I assume the FreeRTOS sources are quite well debugged.

Now and then I notice that there is no call stack at all, it just stops at an interrupt.

I work with SDK 2.10.0.

Any ideas?

0 项奖励
回复
1 解答
2,754 次查看
Daan
Contributor III

Thanks for the reply.

I switched to the Segger driver for the debugger, this resolved my problem, I don't get the hardfaults on power-up any more.

Regards,

Danny

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,664 次查看
Daan
Contributor III

It seems that the hardfaults are caused by an incorrectly written flash, as mentioned before, I need to reflash the application, if I then inspect the console output, I noticed that 1 sector (of 12) is rewritten, that's odd, since the code has not changed. Is there some way to verify the flash during or after programming?

0 项奖励
回复
2,755 次查看
Daan
Contributor III

Thanks for the reply.

I switched to the Segger driver for the debugger, this resolved my problem, I don't get the hardfaults on power-up any more.

Regards,

Danny

0 项奖励
回复
2,827 次查看
Daan
Contributor III

Okay thank you, I'll install the latest SDK.

Regards,

Daan

0 项奖励
回复
2,828 次查看
Daan
Contributor III

Okay thank you, I'll install the latest SDK.

0 项奖励
回复
2,830 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Daan,

The random nature of the issue that you are describing makes it difficult to pinpoint the error to something specific. However, many bug fixes come with each release of our SDKs, so the first recommendation would definitely be to update the SDK to the latest release (2.12.0 as of now). Let me know if the problem persists after this.

 

BR,

Edwin.

0 项奖励
回复