Freescale official Linux Release BSP build with YOCTO.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale official Linux Release BSP build with YOCTO.

1,468件の閲覧回数
sujithvasudevan
Contributor II

Can somebody help me build - freescale official Release BSP  with YOCTO.

The steps i followed  is as below.  Please correct me if i am wrong.

1. Downloaded fsl-L3.14.28_1.0.0_iMX6qdls_Bundle.tar

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

2. Untared fsl-L3.14.28_1.0.0_iMX6qdls_Bundle.tar which had two files in it fsl-yocto-3.14.28-1.0.0.tar.gz and L3.14.28_1.0.0_ga_images_MX6.tar.gz .

3. Untared fsl-yocto-3.14.28-1.0.0.tar.gz and followed steps in the document Freescale_Yocto_Project_User's_Guide.pdf

   

At end of it i am looking to get a u-boot image with version v2014.04.

-

warm regards,

Sujith Vasudevan

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,073件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Your understanding is correct. What is the problem now ?

"After a build is complete, the created image resides in <build directory>/tmp/deploy/images."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,073件の閲覧回数
sujithvasudevan
Contributor II

Thank You Yuri,

This post was made with reference to resolve issue in the following thread:

Re: kernel hangs @ Starting kernel ...

Following the procedure mentioned above the U-boot boots with the following message

U-Boot 2014.10+fslc+g5fd0b60 (Oct 28 2015 - 10:27:43)

CPU:   Freescale i.MX6Q rev1.0 at 792 MHz

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

The release note mentions u-boot version 2014.04 ,  but the image i build boots with version 2014.10+fslc+g5fd0b60. 

warm regards

Sujith Vasudevan

0 件の賞賛
返信