Dear imx community,
I have tried with demo image with imx25 board for ts_calibration to check my board touchscreen functionality is working or not.
while booting up the demo image during the boot process it will ask the user to touch the screen for touch screen calibration even i touched that there is no response from screen on terminal
the terminal message is like and also gnome desktop is not coming on screen. please give the soltion to resolve this issue.
i cant get the freescale login also . it is like below in terminal...
-------
xres = 640, yres = 480 | |
Failed to get root pixmap id | |
matchbox-panel: creating //.matchbox directory for session files | |
matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None ) | |
matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( None ) | |
user_overides is (nil) | |
mb-desktop-dotdesktop: failed to open /usr/local/share/applications | |
mb-desktop-dotdesktop: failed to open //.applications | |
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name | |
mb-applet-menu-launcher: failed to open /usr/local/share/applications | |
mb-applet-menu-launcher: failed to open //.applications | |
mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name | |
mb-applet-menu-launcher: failed to open /usr/local/share/applications |
mb-applet-menu-launcher: failed to open //.applications
---------
Regards,
Guru
Solved! Go to Solution.
Yixing, Thank you for tracking this issue. the problem has been solved . the problem is in connector.there is some lose contact.
Regards,
Guru
Guru, our engineer is contacting you and asking you question. please respond to the question as soon as possible. If your issue had been resolved or no long exists, please click Correct Answer/Helpful Answer in 3 days.
Thanks,
Yixiing
Yixing, Thank you for tracking this issue. the problem has been solved . the problem is in connector.there is some lose contact.
Regards,
Guru
Have you tried hitting the carriage return on the terminal.
Best regards,
-Mahesh