Dear imx community,
I have tried with demo image with imx25 board for ts_calibration to check my board touchscreen functionality is working or not.
while booting up the demo image during the boot process it will ask the user to touch the screen for touch screen calibration even i touched that there is no response from screen on terminal
the terminal message is like and also gnome desktop is not coming on screen. please give the soltion to resolve this issue.
i cant get the freescale login also . it is like below in terminal...
-------
| xres = 640, yres = 480 | |
| Failed to get root pixmap id | |
| matchbox-panel: creating //.matchbox directory for session files | |
| matchbox-desktop: loading /usr/lib/matchbox/desktop/tasks.so with args ( None ) | |
| matchbox-desktop: loading /usr/lib/matchbox/desktop/dotdesktop.so with args ( None ) | |
| user_overides is (nil) | |
| mb-desktop-dotdesktop: failed to open /usr/local/share/applications | |
| mb-desktop-dotdesktop: failed to open //.applications | |
| mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name | |
| mb-applet-menu-launcher: failed to open /usr/local/share/applications | |
| mb-applet-menu-launcher: failed to open //.applications | |
| mb-applet-menu-launcher: bonobo-browser.desktop has no icon, png or name | |
| mb-applet-menu-launcher: failed to open /usr/local/share/applications | |
mb-applet-menu-launcher: failed to open //.applications
---------
Regards,
Guru