Freescale iMX6Q-SABRESD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale iMX6Q-SABRESD board

1,400 Views
mchavva
Contributor I

I would like to build the demo application either android or linux for this board. I downloaded fsl-yacto-3.14.28-1.0.0.tar.gz and following the instructions as per Freescale_Yacto_project_user's_guide.pdf. I do have fsl-release-bsp and downloaded the linux from git. However when I run the "bitbake fsl-image-gui", I run into a serious of non-working links. I downloaded the packages manually as they are the older versions and the links have newer versions for the same packages. However I cannot find fsl-gpu-sdk-2.0.1.bin file and gst1.0-fsl-plugins-4.0.3.tar.gz file to download manually.

Where can I find these files to download?

Thanks a lot.

Here is the error message I get  -

NOTE: Executing RunQueue Tasks

WARNING: Checksum failure encountered with download of http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//fsl-gpu-sdk-2.0.1.bin;fsl-eula=true - will attempt other sources if available

WARNING: Renaming /home/data/freescale/fsl-release-bsp/downloads/fsl-gpu-sdk-2.0.1.bin to /home/data/freescale/fsl-release-bsp/downloads/fsl-gpu-sdk-2.0.1.bin_bad-checksum_c32ad802df5abca941d784abf642e7fd

WARNING: Checksum failure encountered with download of http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//gst1.0-fsl-plugins-4.0.3.tar.gz - will attempt other sources if available

WARNING: Renaming /home/data/freescale/fsl-release-bsp/downloads/gst1.0-fsl-plugins-4.0.3.tar.gz to /home/data/freescale/fsl-release-bsp/downloads/gst1.0-fsl-plugins-4.0.3.tar.gz_bad-checksum_c32ad802df5abca941d784abf642e7fd

ERROR: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//gst1.0-fsl-plugins-4.0.3.tar.gz'. Checksum mismatch!

File: '/home/data/freescale/fsl-release-bsp/downloads/gst1.0-fsl-plugins-4.0.3.tar.gz' has md5 checksum c32ad802df5abca941d784abf642e7fd when b5c1072536479c174bda1349ade5d10c was expected

File: '/home/data/freescale/fsl-release-bsp/downloads/gst1.0-fsl-plugins-4.0.3.tar.gz' has sha256 checksum 538f31569367cebb992643e46213f223fc20113e63a2e814a1dcb64a858ffb2e when 9d5c051cbde023014e67fde07bc314b6b9a5e7030e24eb0d8afdf33e7e458125 was expected

If this change is expected (e.g. you have upgraded to a new version without updating the checksums) then you can use these lines within the recipe:

SRC_URI[md5sum] = "c32ad802df5abca941d784abf642e7fd"

SRC_URI[sha256sum] = "538f31569367cebb992643e46213f223fc20113e63a2e814a1dcb64a858ffb2e"

Otherwise you should retry the download and/or check with upstream to determine if the file has become corrupted or otherwise unexpectedly modified.

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//gst1.0-fsl-plugins-4.0.3.tar.gz'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/data/freescale/fsl-release-bsp/imx6qsabresd/tmp/work/imx6qsabresd-poky-linux-gnueabi/gst1.0-fsl-plugin/4.0.3-r0/temp/log.do_fetch.30362

ERROR: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//fsl-gpu-sdk-2.0.1.bin;fsl-eula=true'. Checksum mismatch!

File: '/home/data/freescale/fsl-release-bsp/downloads/fsl-gpu-sdk-2.0.1.bin' has md5 checksum c32ad802df5abca941d784abf642e7fd when bf79f40f178c3614e40860a3ccfda00c was expected

File: '/home/data/freescale/fsl-release-bsp/downloads/fsl-gpu-sdk-2.0.1.bin' has sha256 checksum 538f31569367cebb992643e46213f223fc20113e63a2e814a1dcb64a858ffb2e when 237196ffbee7adb493ffd107fb392c6f3047c9ffc49c024787c4a2a7b92c65a5 was expected

If this change is expected (e.g. you have upgraded to a new version without updating the checksums) then you can use these lines within the recipe:

SRC_URI[md5sum] = "c32ad802df5abca941d784abf642e7fd"

SRC_URI[sha256sum] = "538f31569367cebb992643e46213f223fc20113e63a2e814a1dcb64a858ffb2e"

Otherwise you should retry the download and/or check with upstream to determine if the file has become corrupted or otherwise unexpectedly modified.

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//fsl-gpu-sdk-2.0.1.bin;fsl-eula=true'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/data/freescale/fsl-release-bsp/imx6qsabresd/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/fsl-gpu-sdk/2.0.1-r0/temp/log.do_fetch.30361

ERROR: Task 1388 (/home/data/freescale/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-graphics/fsl-gpu-sdk/fsl-gpu-sdk_2.0.1.bb, do_fetch) failed with exit code '1'

ERROR: Task 1362 (/home/data/freescale/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-multimedia/gstreamer/gst1.0-fsl-plugin_4.0.3.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2192 tasks of which 2189 didn't need to be rerun and 2 failed.

Labels (1)
0 Kudos
Reply
1 Reply

550 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please try the following patch release.

http://cache.freescale.com/files/32bit/doc/support_info/IMX6L31428101RN.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply