Freescale git out of commission.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale git out of commission.

947件の閲覧回数
le-cherng_yong
Contributor I

Hi there

I was maintaining an old project which use the imx6 yocto repo. I found that the old freescale git has be out of commission and replace with source.codeaurora and this impact one of the bb file in the 

firmware-imx.inc\firmware-imx\recipes-bsp\meta-bsp\imx - meta-fsl-bsp-release - i.MX Yocto Project R... 

which still pointing to the old freescale git. Can you help to update it to point to the new git source?

Thanks

Yong

タグ(1)
0 件の賞賛
返信
1 返信

901件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yong,

My apologies for the inconveniences this is causing. As you pointed out the git://git.freescale.com repository was decommissioned, and its contents were moved to the following repositories:

github.com/NXP

github.com/NXPMicro

https://source.codeaurora.org/external/imx/

As for the imx-firmware packages in particular, the firmware-imx GIT repository new location is:

https://github.com/NXP/imx-firmware

I hope this helps!

Regards,

0 件の賞賛
返信