I am trying to build a live video streaming embedded server on Freescale imx6 with Gstreamer and h264 codecs. The client(Linux PC) is connected via a wireless link that streams the video transmitted by the server.
Recently I performed some test to measure the average bitrate for a h264 encoded file on a Freescale imx6 processor. I used the GStreamer element 'testvideosrc', ran it for 60 seconds and encoded it using the gstreamer-imx plugins that utilizes the hardware encoder (h264) and saved the file, and calculated the bitrate. Following is the command :
timeout --signal=SIGINT 60s \
gst-launch-1.0 -ev videotestsrc pattern=18 ! \
video/x-raw,width=100,height=50,framerate=10/1 ! \
imxvpuenc_h264 bitrate=5 ! h264parse ! \
filesink location=60s.h264 && \
echo $(( $(stat --format=%s 60s.h264) / 60 * 8)) The test was performed at 10 fps for different resolutions, and the bitrates are as follows:
Resolution BitRate
100 x 50 ~120.3K
320 x 240 ~93.7K
640 x 480 ~52.7K
1280 x 960 ~32.3K The bitrate I calculated was for the file transfer rate, that I require to transfer this wirelessly over the communication link.
I am trying to understand the behaviour of the H264 encoder, as to why the bitrate is inversely proportional to the increasing resolution sizes. I had hoped that with increasing resolutions, the bitrate will also increase and hence was opting for a lower resolution image, for streaming through the wireless link. Can anyone explain, why this behaviour exists with the h264 codedc? Or am I at fault in understanding the bitrate demand.
Here is the file-size of the encoded video file.
Resolution File size in bytes
100 x 50 3886780
320 x 240 704543
640 x 480 397098
1280 x 960 235108Could anyone explain this behaviour?
Please address this question to the H264 encoder experts, who can explain this behaviour.
Hello,
Any updates for this question?
Regards.
Hello Joan,
Here are more numbers at different framerates:
at 30 fps
Resolution File size in bytes Bitrate
100 x 50 3474013 455.16K
320 x 240 692716 92.36K
640 x 480 397563 53.01K
1280 x 960 234252 31.23K
at 60 fps
Resolution File size in bytes Bitrate
100 x 50 3470160 425.43K
320 x 240 703225 93.76K
640 x 480 399125 53.216K
1280 x 960 233787 31.168K
I do not understand "the real frame rate". How do I check this?
Regards.