Freescale DDR3 script for MT41K256M16TW-107

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale DDR3 script for MT41K256M16TW-107

Jump to solution
1,022 Views
george
Senior Contributor II

Dear, Yuri

Even the newest Script Aid does not have setting for DDR3-1866.

i.MX6DQSDL DDR3 Script Aid 

When choosing DDR3-1066 using this script, which value is used from memory the data sheet?

* The memory to be used is MT41K256M16TW-107.

pastedImage_5.png

or

pastedImage_7.png

Best Regards,

Fukutomi

0 Kudos
Reply
1 Solution
762 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Use memory Datasheet parameters for DDR3L-1066. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

0 Kudos
Reply
2 Replies
763 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

    Use memory Datasheet parameters for DDR3L-1066. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply
762 Views
george
Senior Contributor II

Thanks,

Fukutomi

0 Kudos
Reply