FreeRtos package for M4 on i.mx8M Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRtos package for M4 on i.mx8M Mini

ソリューションへジャンプ
1,207件の閲覧回数
matt67
Contributor III

Hello,

Where can i Find the FreeRTOS package with example and hardware HAL for M4 on i.mx8M Mini ?

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
1,064件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

FreeRTOS examples are included on the MCUXpresso SDK, which could be downloaded from the link below, choosing the i.MX8M Mini as selected target:

https://mcuxpresso.nxp.com/en/select 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,065件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

FreeRTOS examples are included on the MCUXpresso SDK, which could be downloaded from the link below, choosing the i.MX8M Mini as selected target:

https://mcuxpresso.nxp.com/en/select 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信
1,064件の閲覧回数
matt67
Contributor III

Thank you

0 件の賞賛
返信