FreeRTOS .text area in IMX7D-M4 TCM memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeRTOS .text area in IMX7D-M4 TCM memory

1,524 次查看
andreas_vorderl
Contributor I

Hi,

I have searched a lot but I did not find a good answer if it is possible to store code of FreeRTOS on the Cortex-M4 internal memory TCM_L and TCM_H together.

So my question is, is it possible to store code on both memory areas without splitting them in the tcm.ld memory definition file? Can I use them as one memory area? In FreeRTOS I can define a .text area which is mapped to a defined memory area of the tcm.ld file.
Does this cause failures if instructions are stored over the area of TCM_L and TCM_H?


Thanks in advance for your reply.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,372 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Andreas:

TCM_L is on  Code Bus, to Flash and to Code SRAM

TCM_H is on System Bus, to stack SRAM and to Periperals.

I think it is not good to store FreeRTOS code on both memory areas.

pastedImage_1.png

Regards

Daniel

0 项奖励
回复

1,372 次查看
andreas_vorderl
Contributor I

Hi Daniel,

thanks for the quick response.

Do you mean it is not a good idea to store them on both memory maps because of unpredictable processor behaviour?
Or do you have other Concerns?

Best Regards,

Andreas

0 项奖励
回复