FreeRTOS .text area in IMX7D-M4 TCM memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS .text area in IMX7D-M4 TCM memory

1,565件の閲覧回数
andreas_vorderl
Contributor I

Hi,

I have searched a lot but I did not find a good answer if it is possible to store code of FreeRTOS on the Cortex-M4 internal memory TCM_L and TCM_H together.

So my question is, is it possible to store code on both memory areas without splitting them in the tcm.ld memory definition file? Can I use them as one memory area? In FreeRTOS I can define a .text area which is mapped to a defined memory area of the tcm.ld file.
Does this cause failures if instructions are stored over the area of TCM_L and TCM_H?


Thanks in advance for your reply.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,413件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Andreas:

TCM_L is on  Code Bus, to Flash and to Code SRAM

TCM_H is on System Bus, to stack SRAM and to Periperals.

I think it is not good to store FreeRTOS code on both memory areas.

pastedImage_1.png

Regards

Daniel

0 件の賞賛
返信

1,413件の閲覧回数
andreas_vorderl
Contributor I

Hi Daniel,

thanks for the quick response.

Do you mean it is not a good idea to store them on both memory maps because of unpredictable processor behaviour?
Or do you have other Concerns?

Best Regards,

Andreas

0 件の賞賛
返信