Frames are getting dropped on repeated playback

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frames are getting dropped on repeated playback

2,019件の閲覧回数
ramakrishnakama
Contributor I

Video property is as follows :

Topology:

container: Audio Video Interleave (AVI)

audio: MPEG-1 Layer 3 (MP3)

video: ITU H.264

Properties:

Duration: 1:03:59.059562500

Seekable: yes

Tags:

video codec: ITU H.264

audio codec: MPEG-1 layer 3

encoder: MEncoder SVN-r29352(20090610-gcc4.3.3)

container format: AVI

nominal bitrate: 128000

has crc: false

channel mode: joint-stereo

bitrate: 128000

We are using aiurdemux, vpudec and mfw_v4lsink.

Our Pipeline

gst-launch=0.10 filesrc location=/mnt/usb/Visteon_800_480_1.avi typefind=true !

aiurdemux name=demux demux. ! queue ! vpudec ! mfw_v4lsink demux. ! queue !

beepdec ! audioconvert ! alsasink

It is not reproducing always. On repeated playback we observed sometimes.

We have observed same behavior with playbin2 also.

File size is too big, So not able to attach here. If required we will upload file in FTP.

We are using gst-fsl-plugins version 3.5.7 and gstreamer version 10.36

Result of "uname -a" is

Linux freescale 3.0.35-2154-g94689e1 #180 SMP PREEMPT Wed Mar 4 15:24:49

CST 2015 armv7l GNU/Linux

BSP version is 3.0.35 based customized BSP.

Board is IM6D based customized board .

This is very urgent, for a production program. SOP is very close.

Please help us analysing this ASAP.

Regards:

Ramakrishna Kamath

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,834件の閲覧回数
ramakrishnakama
Contributor I
0 件の賞賛
返信

1,834件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I have consulted with the experts, and it would be required the specific file and configuration that you have used. Additionally, it could be better if there is available an “always reproducible” procedure. Did you was able to upload file to any other server?

Best regards!

/Carlos

0 件の賞賛
返信

1,834件の閲覧回数
ramakrishnakama
Contributor I

Hi Carlos,

Currently we don't know, how to reproduce this issue always.

We are able to reproduce with playbin. So it is not related to our configuration.

Only steps we knew to reproduce is playing video with playbin.

If it plays fine, stop and retry to play.

We have uploaded log and file in Our FTP server at path: "/data/From_Allgo_To_FSL/354686/Frame Drop in Vpudec .tar.bz2"

HI jackmao

Please help Carlos to get file from FTP.

Thanks and Regards,

Ramakrishna Kamath

0 件の賞賛
返信

1,834件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I mailed to you many times for this issue, could you give me any reply for the SR? thanks.

0 件の賞賛
返信