Framebuffer rotation 90 degrees

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Framebuffer rotation 90 degrees

2,237 次查看
jamalmohiuddin
Contributor III

Hi Guys,

We have an application running on customized i.MX6 using DirectFB for displaying images.

We now have a requirement of converting to portrait mode, currently the LCD is in landscape mode.. So , we want the image to be displayed 90 degrees rotated.

DirectFB only supports 180 degree rotation, If i pass "layer-rotate=90" or "layer-rotate=270", it throws error: "UNIMPLEMENTED".

I tried the rotation example from IPU examples, but it was rotating one image.. Now suppose if I want to use this IPU code and add it into the DirectFB for frame buffer rotation of 90 degrees.

标签 (4)
标记 (1)
0 项奖励
回复
1 回复

1,693 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复