Frame grab from mfw_isink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frame grab from mfw_isink

2,729 Views
TalleyHo
Contributor II

I'm looking to capture a snapshot of a running video.  My sink is mfw_isink.  When requested, I grab the last-buffer from the sink and store it to a file.  

 

So.... 

gst-launch playbin2 uri=uri video-sink=mfw_isink

 

From code:

g_object_get(G_OBJECT(m_vsink), "last-buffer", &buffer, NULL);

 

The following caps come from the buffer:

Caps video/x-raw-yuv, format=(fourcc)NV12, width=(int)720, height=(int)480, width_align=(int)64, height_align=(int)64, framerate=(fraction)30000/1001, pixel-aspect-ratio=(fraction)4/3, crop-top-by-pixel=(int)0, crop-left-by-pixel=(int)0, crop-right-by-pixel=(int)48, crop-bottom-by-pixel=(int)32, num-buffers-required=(int)10, field=(int)0

Last buffer size: 589824

Last buffer timestamp: 0:00:05.068854819


 

 

My confusion and concerns stem from the num-buffers-required field.  When I try to use the IPU unit test to convert, the resulting file doesn't appear to be a full frame.  The buffer size also doesn't seem to match up w/ what I expected size wise.  I can tell what was supposed to be on screen, but it certainly isn't exactly what was on screen.  It also doesn't look like it is only 1/10th of the screen either.  What I find interesting, is that the actual video on screen is not equal to the caps provided.

 

When running this on the PC using Xvimagesink, the last-buffer field provided a full frame.  Shouldn't this be the case here?  If not, how would I go about getting a full screen grab of a running video?

 

Mx53/BSP 11.05

Tags (1)
5 Replies

2,260 Views
KanHU
Contributor III

you can set fmt property of mfw_vpudecoder, 0 for NV12, 1 for I420. if you need other format, you need other csc plugin, like mfw_ipucsc.

0 Kudos
Reply

2,260 Views
TalleyHo
Contributor II

I'll put a caps in place to force the format.  I've been using playbin2.  I haven't found a method to how it picks the format.

The resulting image is black and white.  However, there are 'green' borders around the right/bottom side.  Even the ipu unit test won't decode it properly.  Or, at least, I haven't found the correct parameters to give it to decode it correctly.  I ultimately need it ARGB/32 format.

0 Kudos
Reply

2,260 Views
KanHU
Contributor III

you mean the image grabbed is back and white? it looks like you get the wrong u,v data.

the I420 and NV12 are all 4:2:0 YUV data. the difference is that I420 is U, V planar and NV12 is UV interleave means like UVUV. 

take I420 as example, the u, v area also has cropped field which crop-left/right, crop-top/bottom is half of Y.

I'm not sure imagemagic can process NV12 format, if you use mfw_vpudecoder before mfw_isink , you can set fmt property of mfw_vpudecoder for switch vpu outformat from NV12 to I420.

0 Kudos
Reply

2,260 Views
TalleyHo
Contributor II

Hi Kan,

  Thanks for the suggestion.  The cropping explains the strangeness in gimp.  However, I get color banding on the bottom/right sides (maybe the cropped area, not sure) and the images are in black and white.  

I'm using imagemagic to convert: convert -size 768x512 -sampling-factor 2x2 -depth 8 /nfsshare/screenshot.yuv (displayed image is 720x480, with 48/32 cropping areas)

What else is necessary?  The format changes NV12/I420 depending on what source is decoding, but that doesn't seem to have any bearing on the resulting image.  Other than the cropping area, doing the exact same thing w/ xvimagesink produces a nice snapshot.

0 Kudos
Reply

2,260 Views
KanHU
Contributor III

one gstbuffer will contain whole frame including crop area.

the buffersize is calculated for (width+crop-left-by-pixel+crop-right-by-pixel)*(height+crop-top-by-pixel+crop-bottom-by-pixel)*1.5 for 12 bits per pixel of NV12 format.

 

If you need grab the snapshot, you need also eliminate  the crop area

0 Kudos
Reply