Frame data shift issue while Integrating SE3300 Scan Engine with IMX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frame data shift issue while Integrating SE3300 Scan Engine with IMX25

1,503 Views
priti1z
Contributor II


Hi All,

I am trying to integarte a SE3300(Sensor from motorola) with Imx25 through CSI interface.This sensor is 752x480 WVGA.I am facing frame data shift issue.After debugging i found if i set DMA BURST SIZE = 4 and RXFIFO = 96 ,i am not seeing the data shift issue in snap shot mode but with video mode there is always 2nd frame is shifted,

Apart from the mentioned settings ,none of the combination of these settiings works even in snap shot mode.

PFA the problem statement.

Please Help me on this.

Regards,

Priti

0 Kudos
Reply
1 Reply

1,326 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.