Frame buffer resolution in i.Mx6 Yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Frame buffer resolution in i.Mx6 Yocto

2,270件の閲覧回数
MuhammadhSalih
Contributor I

Hi,

I am using i.Mx6Q processor with the Yocto BSP release of fsl-yocto-L3.14.38_6qp-ga (imx-3.14.38-6QP_ga). I have tried to Launch the Yocto filesystem in my customized platform with GUI in my LCD-display (800x480). While dumping any image into it, the image is not properly visible.

I have found that there is a change in the virtual X/Y resolution of display. Below is the command executed to check the same:

root@board:~#

root@board:~# fbset

mode "800x480-60"

    # D: 33.260 MHz, H: 31.496 kHz, V: 59.993 Hz

    geometry 800 480 832 512 16

    timings 30066 88 40 33 10 128 2

    rgba 5/11,6/5,5/0,0/0

endmode

root@board:~#

Here the virtual X/Y resolution is increased by 32 (832 512) instead of (800 480).

Is it even number aligned resolution?. Please suggest me to solve this issue.

Regards,

Salih

ラベル(5)
0 件の賞賛
返信
1 返信

1,468件の閲覧回数
b36401
NXP Employee
NXP Employee

You can change virtual resolution with the command like this:

# fbset -vxres 800 -vyres 480

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信