Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

915 次查看
jw216
Contributor I

Fow what value i can set as following TBD, in MX8M_LPDDR4_RPA_v24.xlsx file ,when I want set 1866MHZ,thanks and best regards

memory set0x3036006832TBD#HW_DRAM_PLL_CFG2_ADDR: For 1866MHz DDR speed, Configure DRAM PLL for 933MHz operation
0 项奖励
回复
1 回复

849 次查看
igorpadykov
NXP Employee
NXP Employee

Hi charles

in general "TBD" values can be left in default state.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复