Customer: Foryou
Platform: i.MX8QXP + QNX
Issue:
Customer wants to change SCFW_BUILD and SCFW_COMMIT in scfw, but failed.
I tried to change it in platform\main\build_info.h,
#ifndef BUILD_INFO_H
#define BUILD_INFO_H
#define SCFW_BRANCH imx_4.14.98_2.0.0_ga
#define SCFW_BUILD 1122UL
#define SCFW_COMMIT 0x33445566UL
#define SCFW_DATE "Apr 20 2020"
#define SCFW_DATE2 Apr_20_2020
#define SCFW_TIME "16:47:37"
#endif
but uboot still get old scfw info:
BuildInfo:
- SCFW a5df0112, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF 30d73be
- U-Boot 2018.03-00013-g0d6d880779-dirty
can it be changed by customer?
Thanks,
Lambert
Solved! Go to Solution.
Yes, it can't be changed by customer, the build information is fixed in NXP binary code of SCFW porting kit.
Yes, it can't be changed by customer, the build information is fixed in NXP binary code of SCFW porting kit.