For imx8m mini Android 10 OS where can i disable HDMI in imx8m mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For imx8m mini Android 10 OS where can i disable HDMI in imx8m mini

1,200 Views
Ruban1
Contributor II

For imx8m mini Android 10 OS where can i disable HDMI in imx8m mini

i am not able to find imx8mm-hdmi.dts find..which dts file i have to disable HDMI to enable LVDS using SN65DSI83 MIPI-to-LVDS

Labels (1)
0 Kudos
2 Replies

1,183 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the i.MX8MM only support the MIPI DSI, we have the MIPI DSI to HDMI board connect to the EVK board.

 You can see the display , you do not need to disable it:

&mipi_dsi {
status = "okay";
 
port@1 {
dsim_to_adv7535: endpoint {
remote-endpoint = <&adv7535_from_dsim>;
attach-bridge;
};
};
};
in the imx8mm-evk.dtsi.
For MIPI DSI to LVDS display you need to modify the remote-endpoint.
And configure the adv_bridge according to your dsiplay:
adv_bridge: adv7535@3d {
compatible = "adi,adv7533";
reg = <0x3d>;
adi,addr-cec = <0x3b>;
adi,dsi-lanes = <4>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2_synaptics_dsx_io>;
interrupt-parent = <&gpio1>;
interrupts = <9 IRQ_TYPE_LEVEL_LOW>;
 
status = "okay";
 
port {
adv7535_from_dsim: endpoint {
remote-endpoint = <&dsim_to_adv7535>;
};
};
};
0 Kudos

1,178 Views
Ruban1
Contributor II

I have attached my function below.

-> Why attach-bridge is used is used in mipi-dsi function inside port1.

-> Should i replace my my lvds to port 1 or its fine in port 2 also

I have attached screenshot of i2c detect

i have added sn65dsi83 driver in i2c detect for prebuild image i am able to see the slave address 2c. after added the fuction in dts and driver file .

It shows as UU.

-> what is the difference between display slave address and display UU.

I have added driver folder below

-> I have only edited in .dts file and added driver. Should i even edit in any other file also.

And should i config in drm/panel any files in panel folder tomatch to the display or only in .dts file is enough.

Kindly address to every question above.

Thanks and Regards

Ruban

Tags (1)
0 Kudos