I have attached my function below.
-> Why attach-bridge is used is used in mipi-dsi function inside port1.
-> Should i replace my my lvds to port 1 or its fine in port 2 also
I have attached screenshot of i2c detect
i have added sn65dsi83 driver in i2c detect for prebuild image i am able to see the slave address 2c. after added the fuction in dts and driver file .
It shows as UU.
-> what is the difference between display slave address and display UU.
I have added driver folder below
-> I have only edited in .dts file and added driver. Should i even edit in any other file also.
And should i config in drm/panel any files in panel folder tomatch to the display or only in .dts file is enough.
Kindly address to every question above.
Thanks and Regards
Ruban