For Ball width tolerance for i.MX6 Dual Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For Ball width tolerance for i.MX6 Dual Lite

Jump to solution
567 Views
yuuki
Senior Contributor II

Dear all,

We design PCB Pad for i.MX6 Dual Lite.

According to the data sheet for i.MX6DL, the tolerance of Ball width is Min:φ0.44 / Typ:φ0.5 / Max:φ 0.65.

However, in the data sheet gor i.MX6Q, it is φ0.5+/-0.05. 

Is the Ball width tolerance for i.MX6DL right?

Best Regards,

Yuuki

Labels (1)
0 Kudos
1 Solution
501 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to For Ball Width tolerance for i.MX6 Dual Lite


Have a great day,
Yuri
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
502 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to For Ball Width tolerance for i.MX6 Dual Lite


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos