Flexbuild on imx8mp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbuild on imx8mp

298件の閲覧回数
JasonFSYang
Contributor II

Hi Sirs,

I am using flexbuild to create a debian image for imx8mp,

the command "bld -m imx8mpevk" will automatically build an image that boots from the SD card, however if I want to create a image that boots from the emmc, how can I do ?

I have tried

bld atf -m imx8mpevk -b emmc
bld uboot -m imx8mpevk -b emmc
bld linux
bld bsp -m imx8mpevk
bld boot

to create firmware_imx8mpevk_sdboot.img & boot_IMX_arm64_lts_6.6.36.tar.zst then flash them to the emmc

however, it doesn't work.

Could you help? Thanks

タグ(3)
0 件の賞賛
返信
0 返答(返信)