FlexRAM reconfiguration without ITCM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexRAM reconfiguration without ITCM

740件の閲覧回数
andyteufel
Contributor III

Hi,

I'm working on a board with an RT1010.

I'm trying to configure FlexRAM to use 64 kB of DTCM and 64 kB of OCRAM, with 0 for ITCM. I followed the instructions in this post. My code starts running but it hardfaults shortly after starting, but it does run a bit. I can't seem to be able to debug it beyond that point.

My project is set up using the SDK from Github. It seems that there are some difference in the source files, but I think I managed to do everything the right way (I hope).

I made the following modifications:

To `startup_MIMXRT1011.S`:

 

 

    /* Customized FlexRAM bank configuration at runtime */
    ldr     r0, =0x400ac044     /* Address of register IOMUXC_GPR_GPR17 */
    ldr     r1, =0x000000a5     /* FlexRAM configuration: OCRAM 64 kB (bank 0 and 1), DTCM 64 kB (bank 2 and 3) */
    str     r1, [r0]

    /* Tell the MCU to configure the FlexRAM banks from the register, not from fuses */
    ldr     r0, =0x400ac040     /* Address of register IOMUXC_GPR_GPR16 */
    ldr     r1, [r0]
    orr     r1, r1, #4          /* The 4 corresponds to setting the FLEXRAM_BANK_CFG_SEL bit in register IOMUXC_GPR_GPR16 */
    str     r1, [r0]

    /* Disable ITCM, we are not using it */
    ldr     r0, =0x400ac040     /* Address of register IOMUXC_GPR_GPR16 */
    ldr     r1, [r0]
    and     r1, r1, #0xfffffffe /* Clear INIT_ITCM_EN bit in register IOMUXC_GPR_GPR16: We have configured the ITCM with size 0 */
    str     r1, [r0]

    /* Adjust the DTCM/ITCM sizes */
    ldr     r0, =0x400ac038     /* Address of register IOMUXC_GPR_GPR14 */
    ldr     r1, [r0]
    and     r1, r1, #0xff00ffff /* Clear the ITCM/DTCM size bits in register IOMUXC_GPR_GPR14 */
    orr     r1, r1, #0x00700000 /* Set the bits for DTCM to have size 64 KB */
    str     r1, [r0]

 

 

 

In the function that configures the MPU:

 

 

    /* Region 5 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(5, 0x00000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32B);

    /* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(6, 0x20000000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

    /* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
    MPU->RBAR = ARM_MPU_RBAR(7, 0x20200000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64KB);

 

 

I have attached my linker script as a text file.

I have seen something about a flash driver file (source), but I have no idea what that is or whether that is relevant in my case. I'm not using such a file AFAIK, I am flashing and debugging my device using a JLink.

I'd appreciate any help with this issue.

ラベル(1)
0 件の賞賛
返信
1 返信

688件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well. I will gladly help you with this.

I suggest you using the most recent SDK version from the SDK builder: https://mcuxpresso.nxp.com/en/welcome

If there is a request to have 0 kB of any TCM memory, disable the corresponding TCM before setting the size to 0 kB. Use the INT_xTCM_EN fields in the IOMUXC_GPR_GPR16 register to disable the corresponding xTCM memory before configuring it to 0 kB.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信