FlexCAN transceivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN transceivers

1,189 Views
kishorekrish
Contributor I

HI,

I want to implement CAN node for that i have IMX6Q6AVT  soc. I think it already have a FlexCAN controller then i need a CAN transceiver.  so please let me know what are the various types of CAN transceivers supported by your FlexCAN controller,

If any transceiver is support then let me know is driver required for that transceiver or not ???@

Thank you.

0 Kudos
Reply
2 Replies

740 Views
art
NXP Employee
NXP Employee

All common types of CAN transceivers are supported. The most popular and widespread ones seem to be the TJA1050 series transceivers by NXP:

TJA1050|NXP

They do not require any additional software drivers.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

740 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The SABRE_AI_DESIGNFILES board support the CAN module you can refer to it. And here I share a document about the CAN work on our i.MX6Q SabreSD. Hope it can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply