FlexCAN single shot mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexCAN single shot mode

1,894 次查看
madjidlho
Contributor II

Hello,

Single shot mode (also know as one-shot mode) is a transmission mode which will try to send a can frame only once ( no automatic retransmission if there is a transmission error ). For more information about single shot mode you can se SJA1000 manual (http://www.nxp.com/documents/application_note/AN97076.pdf )

We are developing can protocol stacks and in order to implement a time triggered protocol on imx6, we would like to know if single shot feature is available on the can controller.

Thank you for your help.

Best regards,

Madjid

0 项奖励
回复
3 回复数

1,630 次查看
art
NXP Employee
NXP Employee

No, there is no Single Shot Transmission feature implemented in the FlexCAN module of the i.MX6 series processors. Only regular Transmission Abort operation can be performed.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,630 次查看
madjidlho
Contributor II

Hi Artur, thanks for your fast answer.

Do you know if it is possible to detect arbitration lost with flexCan?

thanks for your feedback.

0 项奖励
回复

1,630 次查看
art
NXP Employee
NXP Employee

The FlexCAN module can detect and signal the transmission error.

Best Regards,

Artur

0 项奖励
回复