I'm triyng to setup a CAN interface between my SabreSD board and a CAN viewer from a PC.
Kernel version is 3.0.35, the configuration options of the kernel have not been touched from the repo version.
Nevertheless I've checked that Flexcan is indeed enabled.
The output when booting my system is as follows:
root@imx6qsabresd:~# dmesg | grep can
vcan: Virtual CAN interface driver
flexcan netdevice driver
can: controller area network core (rev 20090105 abi 8)
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
root@imx6qsabresd:~# dmesg | grep CAN
vcan: Virtual CAN interface driver
CAN device driver interface
But no /dev/can0 device exists
Regards
Andoni
HI Andoni
Sabre SD BSP does not support CAN it is supported for Sabre AI boards,
as shown in attached BSP Release Notes for these boards.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor for the info!!
I've looked at this file to make it work (How to enable CAN bus on i.MX6Q SabreSD)
But it seems to be targeted for LTIB.
Do you know how to make it work with yocto?
Regards
Andoni