Flashing i.MX8MPEVK demo image using UUU not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing i.MX8MPEVK demo image using UUU not working

Jump to solution
4,683 Views
deepika_t
Contributor IV

Hi All,

I downloaded demo images L4.14.78_1.0.0_ga_images_MX8MMEVK.zip

SW4 settings are

switch D1  D2    D3   D4
SW4 OFF OFF OFF ON

Attaching the screenshot for the same:

deepika_t_0-1630670757355.png

 

 

dmesg
[77087.606108] usb 1-6: new high-speed USB device number 98 using xhci_hcd
[77087.754953] usb 1-6: New USB device found, idVendor=1fc9, idProduct=0146, bcdDevice= 0.02
[77087.754958] usb 1-6: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[77087.754962] usb 1-6: Product: SE Blank 865
[77087.754964] usb 1-6: Manufacturer: NXP SemiConductor Inc
[77087.757049] hid-generic 0003:1FC9:0146.001F: hiddev2,hidraw3: USB HID v1.10 Device [NXP SemiConductor Inc SE Blank 865 ] on usb-0000:00:14.0-6/input0
deepika@deepika-OptiPlex-3040:~/mfgtools/mfgtools/uuu$ ./uuu L4.14.78_1.0.0_ga_images_MX8MMEVK.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.149-3-gf1c886b

Success 0 Failure 1

Prep 1/ 0 [========> 25% ] Http Download\Uncompress
1:6 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

Can you please let me know the issue.

 

Thanks

Deepika

0 Kudos
Reply
1 Solution
4,630 Views
deepika_t
Contributor IV

HI All,

In the prebuilt binaries there was a uuu.auto.

I tried with uuu.auto and copied the rootfs.wic inside the uuu and added the name of the rootfs file in the uuu.auto.

With this I was able to flash full image

This is for anyone who is stuck.

 

Thanks,

Deepika

View solution in original post

0 Kudos
Reply
4 Replies
4,656 Views
deepika_t
Contributor IV

Hi Igor,

I was going through https://github.com/NXPmicro/mfgtools/issues/183 and came across the term ROM patch

When I flashed the demo image using the uuu tool and loaded u-boot. I gave the following command.

u-boot=> fuse read 0 0
Reading bank 0:

Word 0x00000000: ffafa9eb
u-boot=>

Is there any issue in the board?

Thanks,

Deepika

 

0 Kudos
Reply
4,631 Views
deepika_t
Contributor IV

HI All,

In the prebuilt binaries there was a uuu.auto.

I tried with uuu.auto and copied the rootfs.wic inside the uuu and added the name of the rootfs file in the uuu.auto.

With this I was able to flash full image

This is for anyone who is stuck.

 

Thanks,

Deepika

0 Kudos
Reply
4,662 Views
deepika_t
Contributor IV

Hi Igor,

Thanks for the reply.

The demo image which was shared has been flashed successfully.

I have also built Yocto Image for  i.MX8M Plus EVK using the Yocto project user guide and I followed the following steps. The build was successful

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-hardknott -m imx-5.10.35-2.0.0.xml
$ repo sync

Gave the following command after repo sync
DISTRO=fsl-imx-wayland MACHINE=imx8mpevk source imx-setup-release.sh -b build

With the images inside build/tmp/deploy/images , I tried using uuu for flashing the Yocto built images.

But getting error.

I need to flash the entire multimedia image using the uuu tool.

Is there any document for the same?

Thanks,

Deepika

 

 

0 Kudos
Reply
4,673 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepika

 

recommended to try latest Linux 5.10.9_1.0.0 images as L4.14.78 is outdated release

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Also what board used in the case, as " i.MX8MPEVK demo image" should be used for i.MX8M Plus EVK

and "L4.14.78_1.0.0_ga_images_MX8MMEVK.zip" with i.MX8M Mini EVK.

 

Best regards
igor

0 Kudos
Reply