Flash u-boot-nand.imx to NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash u-boot-nand.imx to NAND

1,829件の閲覧回数
jupiter_hce
Contributor III

Hi,

I am running a customized iMX6ULZ EVK, I am able to use kobs-ng to flash u-boot-nand.imx to NAND in Linux, has anyone used u-boot command to flash u-boot-nand.imx to NAND in u-boot instead? Or is it possible to flash u-boot-nand.imx to NAND in u-boot? Is any iMX6 document to flash u-boot-nand.imx to NAND in u-boot?

Thank you.

- jupiter

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

1,636件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jupiter

nxp does not support such operations in uboot, in general one can look

at mainline uboot resources (sect.7.6. Boot from NAND Flash Memory):

Manual < DULG < DENX 

[U-Boot] [PATCH 3/3] i.MX: nand: add nandbcb update command 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信