Flash and test the newly created EXT4 Partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash and test the newly created EXT4 Partition

1,337件の閲覧回数
vinothkumars
Senior Contributor IV

Dear All,

I created the EMMC Partition with ext4 filesystem type and I planning to flash some data (maybe dummy data.ext4) on that.

Will you please guide me to flash and check the newly created partition in Linux ?

I have some doubts,

1. Do I needs to create any mount point to flash the Userdata in Linux ?

2. Is there any other way to check (flash/write and read) newly created EMMC Partition ?

 

 

 

Regards,
Vinothkumar Sekar
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,329件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vinothkumars,

 

Please note that accordingly to eMMC specifications boot partition size is fixed during production.
Its size is defined in EXT_CSD structure of the eMMC.
So please make sure that you does not touch boot partition during updating partitions, also disabling udev cache.

 

Regards.

 

0 件の賞賛
返信

1,327件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you for the reply @Bio_TICFSL 

I doing the same way. I just adding the partition. To test this partition I have to flash some data.

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信