Fitting a PCIe device to SabreSD causing linux to crash on start up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fitting a PCIe device to SabreSD causing linux to crash on start up

ソリューションへジャンプ
1,734件の閲覧回数
andrewellis
Contributor III

Hi,

 

I have fitted an Amfeltec mPCIe to mPCI adapter to my SabreSD board. When I power the system on uBoot runs normally, and Linux starts to boot, then crashes. I have attached the boot log.

 

I have ensured that the SabreSD and adapter are powered from the same source, I have tried fitting a mPCI card to the adapter and also removing it, and get the same result. I have tried mPCIe cards and Linux boots without any problems, I can then type "lspci" and read information about the card fitted.

 

It seems that Linux does not like the bridge chip. Can someone please suggest how I can resolve this issue.

 

I am using kernel 3.0.35, and Ubuntu downloaded from the Freescale website.

 

Kind regards

 

Andrew

Original Attachment has been moved to: PCIError-log.txt.zip

ラベル(2)
0 件の賞賛
返信
1 解決策
1,253件の閲覧回数
andrewellis
Contributor III

After some help from someone at EBV I found the solution here:

https://community.freescale.com/thread/302251

I hope this helps anyone who comes across this post.

Andrew

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,254件の閲覧回数
andrewellis
Contributor III

After some help from someone at EBV I found the solution here:

https://community.freescale.com/thread/302251

I hope this helps anyone who comes across this post.

Andrew

0 件の賞賛
返信