Finding whether the board is C0 silicon

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Finding whether the board is C0 silicon

Jump to solution
2,346 Views
jaux_al
Contributor I

I have a iMX8QuadXPlus and I set the machine name to imx8qxpmek but when I tried to boot the board off the SD card that contained the yocto image, nothing shows up. 

I'm currently trying out imx8qxpc0mek to see if it works but how else do you determine if your machine is C0 silicon?

0 Kudos
Reply
1 Solution
2,261 Views
igorpadykov
NXP Employee
NXP Employee

also one can look at uboot log

 

Best regards
igor

View solution in original post

0 Kudos
Reply
12 Replies
1,755 Views
_angelo_
Contributor III

Om MEK board,

removed the heatsink CPU has a suffix B at the end of the code

 

CPU PCB BLACK 2017 is b0
CPU PCB GREEN 2018 is c0

0 Kudos
Reply
2,330 Views
jaux_al
Contributor I

But I'm not really migrating from B0 to C0. Just want to understand whether my board is C0 silicon or B0

0 Kudos
Reply
2,325 Views
igorpadykov
NXP Employee
NXP Employee

rev.C0 has suffix "C" of processor marking.

 

Best regards
igor

0 Kudos
Reply
2,315 Views
jaux_al
Contributor I

where can I find that on the EVB board though?

0 Kudos
Reply
2,310 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
2,284 Views
jaux_al
Contributor I

where it does talk about C0 or B0 silicon? I am just trying to get the machine name of my EVB. 

0 Kudos
Reply
2,269 Views
igorpadykov
NXP Employee
NXP Employee

>where it does talk about C0 or B0 silicon?

 

please locate processor on board and look at its marking.

 

Best regards
igor

0 Kudos
Reply
2,266 Views
jaux_al
Contributor I

the only text I see is IMX8-QXP CPU. It has a fan on it so maybe the complete name is hidden underneath, hence my concern about finding the full machine name including the silicon 

0 Kudos
Reply
2,262 Views
igorpadykov
NXP Employee
NXP Employee

also one can look at uboot log

 

Best regards
igor

0 Kudos
Reply
2,257 Views
jaux_al
Contributor I

i have been having issues loading up the yocto image off the SD card. Do you have a sample image of the boot log indicating the silicon type?

0 Kudos
Reply
2,336 Views
igorpadykov
NXP Employee
NXP Employee

Hi jaux_al

 

one can look at AN12770  i.MX 8X C0 Migration Guide Migrating from i.MX 8X B0 to i.MX 8X C0

in particular sect.2.3 Software changes.

 

Best regards
igor

0 Kudos
Reply
2,322 Views
jaux_al
Contributor I

But I'm not looking to migrate between C0 and B0 - just need to know to determine whether my board is C0 or B0

0 Kudos
Reply