Fido5200 with IMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fido5200 with IMX8M

1,260 Views
qphan
Contributor II

Hi,

I have an Analog Devices fido5200 REM switch chip that I would like to use with the IMX8M.  According to their documentation ( https://www.analog.com/media/en/technical-documentation/application-notes/AN-1554.pdf ),  

The fido5100 and fido5200 REM switches connect to a communication processor with a host interface designed as a standard asynchronous memory bus port. The host interface is either a 16-bit or 32-bit memory bus, with the possibility to multiplex address and data, reducing pin count

In the application notes above, they show connections between  fido5200 to the NXP IMX 6ULL processors via External Interface Module (EIM).

Looking at the IMX8M Reference Manual there seems to be a DDR Controller for DDR memories and a GPMI (General Purpose Media Interface) which seems to be for NAND memories.  It seems like there are no controllers/interface on the IMX8M that will work with the fido5200? Can you please confirm my findings?

Thanks,

Quang

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,139 Views
b36401
NXP Employee
NXP Employee

Unfortunately i.MX8M processor does not have EIM.
Sorry for the inconvenience.

0 Kudos
Reply