Ferrite Bead Between VDD_SOC_IN and VDD_ARM_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ferrite Bead Between VDD_SOC_IN and VDD_ARM_IN

Jump to solution
638 Views
markwilliams
Senior Contributor I

Hi, I am just in the final checking stages of our iMX6 board design. The board will take solo, dual or quad processors and has the necessary common hardware design considerations.

We are using a single power supply for the SOC and ARM inputs. In some designs I see people have added a ferrite bead between VDD_ARM_IN and VDD_SOC_IN when feeding from the same supply.

Is this ferrite bead essential? I appreciate it may add some high frequency suppression on the supply line but it seems to just be in the SOC trace.

When routing as an 8-layer board it is nice to add a copper pour to cover both VDD_ARM_IN and VDD_SOC_IN in one, rather than split them into two seperate islands and put a ferrite outside the package area to join them.

Thanks, Mark

0 Kudos
1 Solution
568 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

I agree that with satisfactory board layout ferrite bead is not needed.

Seems purpose is to isolate VDD_ARM_IN island as producing more high

frequency noise.

Best regards
igor
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
569 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

I agree that with satisfactory board layout ferrite bead is not needed.

Seems purpose is to isolate VDD_ARM_IN island as producing more high

frequency noise.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos